Analog Devices ADALM-PLUTO

ADI’s ADALM-PLUTO Active Learning Module (PlutoSDR) is a physical RF lab that fits in the palm of your hand. Its price point and capabilities have made it so popular we are not always able to maintain stock. Key features of the instrument are two independent radio channels, one receive channel, and one transmit channel, which can be operated in full duplex. It can generate or measure RF analog signals from 325 to 3800 MHz.

System Block Diagram

Internal hardware includes the Analog Devices AD9361 RF Agile Transceiver™, Micron DDR3L and QSPI Flash, Xilinx® Zqynq® programmable SoC, and a USB 2.0 PHY. The firmware of the PlutoSDR is open source and uses technology from Das U-Boot, the Linux Kernel, and Buildroot. Detailed schematics, HDL user guide, and documentation can be found on https://wiki.analog.com/university/tools/pluto/developers.

ADALM-PLUTO Capabilities and Use Cases

PlutoSDR was developed to help introduce electrical engineering students to the fundamentals of software-defined radio (SDR), radio frequency (RF), and wireless communications. It is an open and flexible tool intended to support all ranges of users. Students use PlutoSDR to better understand the RF world around them. Developers can write custom software or HDL that runs directly on the open source PlutoSDR platform.

Click here to see Randall Restle’s New Product Discovery video where he talks about the ADALM-PLUTO.

Availability at DigiKey

ADALM-PLUTO  https://www.digikey.com/products/en?keywords=ADALM-PLUTO%20

Related Product Highlights

https://www.digikey.com/en/product-highlight/a/analog-devices/adalm-pluto

Analog Devices Resources

ADI Wiki - ADALM-PLUTO Overview  https://wiki.analog.com/university/tools/pluto

Development Kit Documentation http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/adalm-pluto.html#eb-overview

关于此作者

Image of Scott Raeker

Scott Raeker 是 DigiKey 的首席应用工程师,自 2006 年加入公司以来就一直主要负责协助无线领域的客户。他在电子行业有着超过 35 年的经验,并拥有明尼苏达大学的电气工程学位。业余时间 Scott 喜欢打理他的世纪之交农舍。

More posts by Scott Raeker
 TechForum

Have questions or comments? Continue the conversation on TechForum, Digi-Key's online community and technical resource.

Visit TechForum